JAJSK93 November 2020 TPS27SA08
PRODUCTION DATA
The energy limiting feature is implemented to protect the switch from excessive stress. The device will continuously monitor the amount of energy dissipated in the FET. If the energy limit threshold is reached, the switch will automatically disable. In practice, the energy limit will only be reached during a fault event such as short-to-ground.
Energy limit events have the same system-level behavior as thermal shutdown events.