JAJSOU6 October 2023 TPS2HCS10-Q1
ADVANCE INFORMATION
The following factors should be considered when selecting the RSNS value:
At low current levels, the KSNS factor can be scaled up by a factor of around 4.17 using the configuration bit, OL_ON_EN_CHx, in the DIAG_CONFIG_CHx register to improve the accuracy of current measurement. In order to further improve the resolution at low current levels, the device offers the configuration bit ISNS_SCALE_CHx in the DIAG_CONFIG_CHx register that multiplies the input voltage to the ADC by a factor of 8. This enables the ADC to measure currents even of the order of 10 mA with sufficient bit resolution.