JAJSOU6 October 2023 TPS2HCS10-Q1
ADVANCE INFORMATION
The device includes a battery supply (VBB) under-voltage monitoring. Some of the internal reference and regulators and the output FETs are turned OFF when the VBB supply falls below the VBBUVLOF threshold. When the input VBB supply is lost, the device relies on the low voltage supply input to keep the digital functions and registers alive. The SPI communication is also available as long as VDD input is supplied. The VBB UVLO error fault bits can be read over SPI from the CH_FLT_TYPE_FAULT_GLOBAL_TYPE register (VBB_UVLO bit). The following table indicates the device operation under a loss of supply condition.
VDD < VDD_UVLO | VDD > VDD_UVLO | ||
---|---|---|---|
VBB < VBB_UVLO |
|
|
|
VBB > VBB_UVLO |
|
|
The register information may be lost when both the VBB and VDD supplies are below the POR and UVLO conditions respectively. The device is able to indicate with a register read of the POR bit in the CH_FLT_TYPE_FAULT_GLOBAL_TYPE register that a reset of the digital has occurred. This will ensure that the SPI master can identify that the register contents are all lost and the configuration registers needs to be rewritten. It is recommended that the bit be read if any under-voltage fault is detected