JAJSOU6 October 2023 TPS2HCS10-Q1
ADVANCE INFORMATION
The TPS2HCS10-Q1 includes a temperature sensor on the power FET and also within the controller portion of the device. There are two cases that the device will consider to be a thermal shutdown fault:
After the fault is detected, the switch will turn off. If TJ,FET exceeds TABS, the fault is cleared when the switch temperature decreases by the hysteresis value, THYS. If instead, the TREL threshold is exceeded, the fault is cleared after TRETRY passes.