JAJSFU1A July 2018 – September 2021 TPS3430-Q1
PRODUCTION DATA
The TPS3430-Q1 uses an open-drain configuration for the WDO circuit, as shown in Figure 8-7. When the FET is off, the resistor pulls the drain of the transistor to VDD and when the FET is turned on, the FET attempts to pull the drain to ground, thus creating an effective resistor divider. The resistors in this divider must be chosen to ensure that VOL is below its maximum value. To choose the proper pull-up resistor, there are three key specifications to keep in mind: the pull-up voltage (VPU), the recommended maximum WDO pin current (IWDO), and VOL. The maximum VOL is 0.4 V, meaning that the effective resistor divider created must be able to bring the voltage on the reset pin below 0.4 V with IWDO kept below 10 mA. For this example, with a VPU of 1.8 V, a resistor must be chosen to keep IWDO below 200 μA because this value is the maximum consumption current allowed. To ensure this specification is met, a pull-up resistor value of 10 kΩ was selected, which sinks a maximum of 180 μA when WDO is asserted.