JAJSFN5C November 2014 – February 2019 TPS3701
PRODUCTION DATA.
Figure 21 to Figure 24 show examples of the various input and output configurations.
NOINDENT:
NOTE: The inputs can monitor a voltage higher than VDD (max) with the use of an external resistor divider network.NOINDENT:
NOTE: In this case, OUTA is driven low when an undervoltage condition is detected at the 5-V rail and OUTB is driven low when an overvoltage condition is detected at the 12-V rail.