JAJSGG5D November 2018 – March 2021 TPS3703-Q1
PRODUCTION DATA
Overvoltage and undervoltage comparators include built-in hysteresis that provides noise immunity and ensures stable operation. For example if the voltage on the SENSE pin falls below VIT-(UV) or above VIT+(OV), then RESET is asserted (driven low), then when the voltage on the SENSE pin is between the positive and negative threshold voltages, RESET deasserts after the user-defined RESET delay time. Figure Figure 9-5 shows the relation between VIT-(UV),VIT+(OV) and hysteresis voltage (VHYS).