JAJSCT6B October 2016 – September 2021 TPS3850
PRODUCTION DATA
The TPS3850 features three options for setting the reset delay (tRST): connecting a capacitor to the CRST pin, connecting a pullup resistor to VDD, and leaving the CRST pin unconnected. Figure 8-1 shows a schematic drawing of all three options. To determine which option is connected to the CRST pin, an internal state machine controls the internal pulldown device and measures the pin voltage. This sequence of events takes 381 μs (tINIT) to determine which timing option is used. Every time RESET is asserted, the state machine determines what is connected to the pin.