JAJSHQ7A July 2019 – September 2019 TPS3870-Q1
PRODUCTION DATA.
Another typical application for the TPS3870-Q1 is shown in Figure 25. The TPS3870-Q1 is used in a RESET latch output mode. In latch mode, once RESET driven logic low, it will stay low regardless of the sense voltage. If the RESET pin is low on start up, it will also stay low regardless of sense voltage.