JAJSQQ7 july 2023 TPS38700S-Q1
PRODUCTION DATA
A typical implementation of the sync functionality of the TPS38700S-Q1 is shown in Figure 9-12. TPS38700S-Q1 and TPS389006-Q1 can be used together by tying SYNC pins together in order to ensure that sequential voltage rails are dependent on earlier voltage rails successfully powering up or powering down.
SYNC is an active low input on the TPS38700S-Q1 which causes EN pins to toggle on when sequencing up or off when sequencing down. TPS389006-Q1 will send an active low signal when the desired voltage threshold is monitored. For more information on how sequence logging works and how TPS389006-Q1 tags power rails with SYNC check out the TPS389006-Q1 data sheet.