JAJSQQ7 july 2023 TPS38700S-Q1
PRODUCTION DATA
A similar sequence of events happens when ACT is driven low. Immediately the first EN signal in the down sequence is driven low. This triggers TPS389006-Q1 by having the MON voltage drop below a threshold and send a SYNC signal. The SYNC signal causes TPS38700S-Q1 to turn off the second EN signal. This process also repeats until all voltages have been turned off. By default SYNC voltage thresholds for TPS389006-Q1 are based on the OFF voltage. The voltage thresholds can be changed to UV voltage thresholds for both sequencing up and down. A successful power down sequence is shown in Figure 8-5 using the circuit shown in Figure 9-12. Note that the TPS389006-Q1 defaults to using OFF voltage threshold (MONx<140mV) for sending the SYNC pulse when sequencing down.
Note that TPS38700S-Q1 must finish sequencing (either up or down) before starting a new sequence.