JAJSQQ7 july 2023 TPS38700S-Q1
PRODUCTION DATA
In the TSD state TPS38700S-Q1 reduces functionality to only support I2C commincation. Upon exiting from the TSD state, the last configuration is active and the device enters the SHDN state.
When in BACKUP state, the TPS38700S-Q1 pins are in the following state:
Note that the F_TSD bit in Table 8-4 will be set high. The F_TSD bit will stay high even if TPS38700S-Q1 leaves the TSD state, but can be manually cleared.