JAJSMQ4 june 2023 TPS389006
PRODUCTION DATA
If the sequence overwrite bit is enabled (EN_SEQ_OW=1), the sequence logging registers (SEQ_OFF_LOG[N]) are overwritten with new data. If there was data in the registers that was not read by the host (SEQ_OFF_RDY still set), the sequence overwrite flag (SEQ_OFF_OW) is set.
If the timestamp overwrite bit is enabled (EN_TS_OW=1), the timestamp logging registers (SEQ_TIME_xSB[N]) are overwritten with new data. If there was data in the registers that was not read by the host (TS_RDY still set), the timestamp overwrite flag (TS_OW) is set.
If the sequence overwrite bit is disabled (EN_SEQ_OW=0) and there was data in the registers SEQ_OFF_LOG[N] that was not read and acknowledged by the host (SEQ_OFF_RDY still set), the sequence overwrite flag (SEQ_OFF_OW) is set, and the registers are not overwritten with new data.
If the timestamp overwrite bit is disabled (EN_TS_OW=0) and there was data in the registers SEQ_TIME_xSB[N] that was not read and acknowledged by the host (TS_RDY still set), the timestamp overwrite flag (TS_OW) is set, and the registers are not overwritten with new data.