JAJSLH4B April 2021 – January 2024 TPS3899-Q1
PRODUCTION DATA
The primary constraint for
this application is choosing the correct device to monitor the
supply voltage of the microprocessor. The TPS3899-Q1 can monitor any
voltage with the adjustable voltage threshold option or fixed
voltages between 0.8V and 5.4V. Depending on how far away from the
nominal voltage rail the user wants the voltage supervisor to
trigger determines the correct voltage supervisor variant to choose.
In this example,
Figure 8-2 shows the output, RESET, of the
TPS3899DL01-Q1 when the 3.3V rail falls to 2.9V after the sense time
delay expires. The TPS3899PL16-Q1 triggers a reset when the 1.8V
rail falls to 1.6V.
The secondary constraint
for this application is the sense and reset time delay. If the
monitored voltage rail 3.3V has large voltage ripple noise and goes
below the programmed threshold voltage but returns above the
VIT-+ VHYS
before the sense time delay expires, the output does not assert.
Therefore, the sense time delay prevents false sense resets by
allowing the monitored voltage rail 3.3V to not assert the output
during the programmed sense time delay period set by the capacitor
on the CTS pin. In the application, the CTS capacitors for both the
TPS3899DL01-Q1 and TPS3899PL16-Q1 are set to be 0.022μF and 0.01μF,
respectively, and resulted in sense time delays of 13.7ms and 6.2ms.
In addition to the sense delay time, the reset time delay for the
TPS3899DL01-Q1 must be at least 25ms to allow the microprocessor,
and all other devices using the 3.3V rail, enough time to startup
correctly before the 1.8V rail is enabled via the LDO. Once the LDO
is enabled, the reset time delay for the TPS3899PL16-Q1 must be at
least 10ms to allow the 1.8V rail to settle. For applications with
ambient temperatures ranging from –40°C to +125°C, CTS and CTR can
be calculated using RCTS and RCTR. Solving for
CCTS and CCTR in Equation 4 and Equation 5 for 10ms and 25ms gives a minimum capacitor value of 0.016µF and
0.0403µF which are rounded up to standard values of 0.022µF and
0.047µF, respectively, to account for capacitor tolerance.
A 1µF decoupling capacitor is connected to the VDD pin as a good analog design practice. The pull-up resistor is only required for the open-drain device variants and is calculated to make sure that VOL does not exceed the max limit given the IRESET(Sink) possible at the expected supply voltage. The open-drain variant is used in this design example and the nominal VDD is 3.3V but dropping to 2.9V for VIT-, the voltage across the pull-up resistor can be determined. In Section 6.5, max VOL provides 2mA IRESET(Sink) for 3.3V VDD. Using 2mA of IRESET(Sink) and 300mV max VOL, gives us 1.3kΩ for the pull-up resistor. Any value higher than 1.3kΩ makes sure that VOL does not exceed the 300mV max specification.