JAJSLH4B April 2021 – January 2024 TPS3899-Q1
PRODUCTION DATA
The TPS3899-Q1Voltage supervisor with separate SENSE monitor asserts a RESET/RESET signal when the SENSE pin voltage drops below VIT- for the duration of the sense delay set by CTS. If the SENSE pin voltage rises above VIT- + VHYS before the sense delay expires, the RESET/RESET pin does not assert. When asserted, the RESET/RESET output remains asserted until SENSE voltage returns above VIT- + VHYS for the duration of the reset delay set by CTR. If the SENSE pin voltage falls below VIT- before the reset delay expires while RESET is asserted, RESET/RESET will remain asserted.
Like most voltage supervisors, the TPS3899-Q1 includes a reset delay tD to provide time for the power and clocks to settle before letting the processor out of reset. At power up, the circuits inside the TPS3899-Q1 need additional time to start the reset delay timer after its power supply VDD has reached minimum VDD(MIN) for these circuits to start operating properly. This additional time is specified with the parameter start-up delay tSTRT. Figure 6-1 shows the timing diagram indicating this additional delay. After VDD is stable and above VDD(MIN) subsequent changes of the sense voltage across the threshold voltage will trigger reset after only the reset delay. The reset time delay tD is set by a capacitor on the CTR pin. The start-up delay has a maximum limit of 300μs for a ramp rate of VDD ≤ 1V / μs.