SLVSH18 December 2024 TPS4HC120-Q1
PRODUCTION DATA
In the OFF state, when DIAG_EN is high, there is an internal pull-up resistor ROL that pulls up a channel to VBB. The specific channel that gets pulled up is based on the selection of SEL0 and SEL1, and the other channels do not have the pull-up resistor engaged.
If there is load present at the selected channel, then the output voltage is pulled to around 0V, as the load is much stronger than the ROL. In the case of an open load, the output voltage will be pulled close to the supply voltage by the ROL. If VBB - VOUT < VOL,off for the selected channel, the FLT pin goes low to indicate the fault to the MCU, and the SNS pin is pulled up to ISNSFH.