JAJS311D February 2008 – February 2020 TPS51200
PRODUCTION DATA.
For stable operation, the total capacitance of the VO output pin must be greater than 20 μF. Attach three, 10-μF ceramic capacitors in parallel to minimize the effect of equivalent series resistance (ESR) and equivalent series inductance (ESL). If the ESR is greater than 2 mΩ, insert an RC filter between the output and the VOSNS input to achieve loop stability. The RC filter time constant should be almost the same as or slightly lower than the time constant of the output capacitor and its ESR.