JAJSML7B March 2013 – August 2021 TPS53511
PRODUCTION DATA
TPS53511 uses an adaptive on-time control scheme and does not have a dedicated on-board oscillator. The device runs with a pseudo-constant frequency of 700 kHz by using the input voltage and output voltage to set the on-time one-shot timer. The on time is inversely proportional to the input voltage and proportional to the output voltage. The actual frequency can vary from 700 kHz depending on the off time, which is ended when the fed back portion of the output voltage falls to the VFB threshold voltage.