JAJSKX2A August 2019 – May 2021 TPS53676
PRODUCTION DATA
TPS53676 supports 3 data formats according to the PMBus specification. The data format for each command is listed along with its address and supported values.
TPS53676 accepts writes to SLINEAR11 format commands with any desired exponent value. TI recommends using the default exponent listed for each command for writes to ensure consistent NVM store and restore behavior.
Telemetry commands in the SLINEAR11 format return data with variable exponent values according to the absolute value of the retured value. As a rule TPS53676 returns data in the SLINEAR11 format with the smallest possible exponent, to provide the highest possible command resolution. As a result the host must be able to support decoding of the SLINEAR11 format with any exponent value.