#T5605938-21 shows a conceptual block diagram of the DCAP+ off-time control loop. Transient response tuning is accomplished by changing the parameters which generate the VCOMP signal. These parameters are accessible using the COMPENSATION_CONFIG command. Refer to the Technical Reference Manual for a register map of this command.
The VCOMP signal is generated by the
sum of three signal paths. Finally the VCOMP signal is scaled by the AC
gain parameter, KAC.
- Proportional path: An error amplifier subtracts the
sensed output voltage from the output voltage target, set by
VDAC. The gain of the proportional path is set by the AC load
line (ACLL). Reducing the value of the AC load line increases the
proportional path gain, which gives faster transient response. Setting the
AC load line to a very low value can lead to low phase margin.
- Integral path: The difference between the sensed
output voltage and the output voltage target, VDAC, is compared
to the ideal droop (ISUM × DCLL) value to create an error
voltage, VERR. An integrator adjusts the setpoint of
VCOMP, to drive the output voltage error to zero. Integration
provides high DC gain, giving the power supply excellent output regulation
and DC load line performance. The programmable integration time constant,
τINT changes the settling time of of the output voltage
folliowing a transient. Increasing the integration time constant improves
phase margin. The programmable integration path gain, KINT, sets
the gain of the integral path.
- Current feedback: The summed phase current,
ISUM, with a nominal gain of 5 mV/A, is used directly to
generate VCOMP, as well as in the integral path to set the DC
load line. The gain of this path is not affected by the IOUT_CAL_GAIN or IOUT_CAL_OFFSET calibration commands.