JAJSDK1B May 2017 – March 2018 TPS543B20
PRODUCTION DATA.
PIN | I/O/P(1) | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | RSP | I | The positive input of the remote sense amplifier. Connect RSP pin to the output voltage at the load. For multi-phase configuration, the remote sense amplifier is not needed for slave devices. |
2 | RSN | I | The negative input of the remote sense amplifier. Connect RSN pin to the ground at load side. For multi-phase configuration, the remote sense amplifier is not needed for slave devices. |
3 – 6 | NC | Not connected | |
7 | BOOT | I | Bootstrap pin for the internal flying high-side driver. Connect a typical 100-nF capacitor from this pin to SW. To reduce the voltage spike at SW, a BOOT resistor with a value between 1 Ω to 10 Ω may be placed in series with the BOOT capacitor to slow down turnon of the high-side FET. |
8 – 12 | SW | B | Output of converted power. Connect this pin to the output Inductor. |
13 – 20 | PGND | G | These ground pins are connected to the return of the internal low-side MOSFET |
21 – 25 | PVIN | I | Input power to the power stage. Low impedance bypassing of these pins to PGND is critical. A 10-nF to 100-nF capacitor from PVIN to PGND close to IC is required. |
26 | VDD | I | Controller power supply input |
27 | GND | G | Ground return for the controller. This pin should be directly connected to the thermal pad on the PCB board. A 10-nF to 100-nF capacitor from PVIN to GND close to IC is required. |
28 | BP | O | Output of the 5 V on board regulator. This regulator powers the driver stage of the controller and must be bypassed with a minimum of 2.2 µF to the thermal pad (power stage ground, that is, GND). Low impedance bypassing of this pin to PGND is critical. |
29 | AGND | G | GND return for internal analog circuits. |
30 | ILIM | O | Current protection pin; connect a resistor from this pin to AGND sets current limit level. |
31 | ISHARE | I | Current sharing signal for multi-phase operation. Float this pin for single phase. |
32 | VSHARE | B | Voltage sharing signal for multi-phase operation. Float this pin for single phase. |
33 | EN | I | The enable pin turns on the switcher. |
34 | PGD | O | Open-drain power-good status signal which provides start-up delay after the FB voltage falls within the specified limits. After the FB voltage moves outside the specified limits, PGOOD goes low. |
35 | SYNC | B | For frequency synchronization. This pin can be configured as sync in or sync out by MODE pin and RT pin for master and slave devices. |
36 | VSEL | I | Connect a resistor from this pin to AGND to select internal reference voltage. |
37 | SS | O | Connect a resistor from this pin to AGND to select soft-start time. |
38 | RT | O | Frequency setting pin. Connect a resistor from this pin to AGND to program the switching frequency. This pin also selects sync point for devices in stackable applications |
39 | MODE | B | Enable or disable API or body brake function, choose API threshold, also selects the operation mode in stackable applications |
40 | RAMP | B | Ramp level selection, with a resistor to AGND to adjust internal loop. |
– | Thermal Tab | – | Package thermal tab, internally connected to PGND. The thermal tab must have adequate solder coverage for proper operation. |