8.4.2 Small Signal Model for Frequency Compensation
The TPS54618-Q1 uses a transconductance amplifier for the error amplifier and readily supports two of the commonly used frequency compensation circuits. The compensation circuits are shown in Figure 38. The Type 2 circuits are most likely implemented in high-bandwidth power supply designs using low ESR output capacitors. In Type 2A, one additional high-frequency pole is added to attenuate high-frequency noise.
The design guidelines for TPS54618-Q1 loop compensation are as follows:
- The modulator pole, fpmod, and the esr zero, fz1, must be calculated using Equation 15 and Equation 16. Derating the output capacitor (COUT) may be needed if the output voltage is a high percentage of the capacitor rating. Use the capacitor manufacturer information to derate the capacitor value. Use Equation 17 and Equation 18 to estimate a starting point for the crossover frequency, fc. Equation 17 is the geometric mean of the modulator pole and the esr zero and Equation 18 is the mean of modulator pole and the switching frequency. Use the lower value of Equation 17 or Equation 18 as the maximum crossover frequency.
Equation 15.
space
Equation 16.
space
Equation 17.
space
Equation 18.
space
- R3 can be determined by Equation 19:
Equation 19.
where
- the gmea amplifier gain (245 μA/V)
- gmps is the power stage gain (25 A/V)
vertical spacer
- Place a compensation zero at the dominant pole:
C1 can be determined by Equation 20:
Equation 20.
space
- C2 is optional. It can be used to cancel the zero from the ESR of COUT.
Equation 21.