JAJSQ82B November 2023 – July 2024 TPS548D26
PRODUCTION DATA
For a synchronous buck converter, the inductor current increases at a linear rate determined by the input voltage, the output voltage, and the output inductor value during the high-side MOSFET on-time (ON time). During the low-side MOSFET on-time (OFF time), this inductor current decreases linearly per slew rate determined by the output voltage and the output inductor value. The inductor during the OFF time, even with a negative slew rate, usually flows from the device SW node to the load the device which is said to be sourcing current and the output current is declared to be positive. This section describes the overcurrent limit feature based on the positive low-side current. The next section describes the overcurrent limit feature based on the negative low-side current.
The positive overcurrent limit (OCL) feature in the TPS548D26 device is implemented to clamp low-side valley current on a cycle-by-cycle basis. The inductor current is monitored during the OFF time by sensing the current flowing through the low-side MOSFET. When the sensed low-side MOSFET current remains above the selected OCL threshold, the low-side MOSFET stays ON until the sensed current level becomes lower than the selected OCL threshold. This operation extends the OFF time and pushes the next ON time (where the high-side MOSFET turns on) out. As a result, the average output current sourced by the device is reduced. As long as the load pulls a heavy load where the sensed low-side valley current exceeds the selected OCL threshold, the device continuously operates in this clamping mode which extends the current OFF time and pushes the next ON time out. The device does not implement a fault response circuit directly tied to the overcurrent limit circuit, instead, the VOUT UVF function is used to shuts the device down under an overcurrent fault.
During an overcurrent event, the current sunk by the load (IOUT) exceeds the current sourced by the device to the output capacitors, thus, the output voltage tends to decrease. Eventually, when the output voltage falls below the selected undervoltage fault threshold, the VOUT UVF comparator detects and shuts down the device after the UVF Response Delay (typically 16µs). The device then responds to the VOUT UVF trigger per fault response selected through SS pin. With the Latch-off response selected, the device latches OFF both high-side and low-side drivers. The latch is cleared with a reset of VCC or by toggling the EN pin. With the Hiccup response selected, the device enters hiccup mode and restarts automatically after a hiccup sleep time of 56ms, without limitation on the number of restart attempts. In other words, the response to an overcurrent fault is set by the selected UVF response.
If an OCL condition happens during a soft-start ramp, the device still operates with the cycle-by-cycle current limit based on the sensed low-side valley current. This operation can limit the energy charged into the output capacitors thus the output voltage likely ramps up slower than the desired soft-start slew rate. During the soft start, the VOUT UVF comparator is disabled, thus the device does not respond to an UVF event. Upon the completion of the soft start, the VOUT UVF comparator is enabled, then the device starts responding to the UVF event.
The resistor, RILIM, connected from the ILIM pin to AGND sets the overcurrent limit threshold (see the following table). TI recommends ±1% tolerance resistors with a typical temperature coefficient of ±100 ppm/°C.
ILIM Pin to AGND Resistor (kΩ) | OCL Threshold (Valley Current Detection) |
---|---|
7.5 | 13.4A |
12.1 | 21A |
16.2 | 28.5A |
21.5 | 36.5A |
24.9 | 43A |