JAJSNR4 July 2022 TPS563300
PRODUCTION DATA
Pin | Type(1) | Description | |
---|---|---|---|
Name | NO. | ||
NC | 1 | A | Reserved pin. The user must leave this pin floating. |
EN | 2 | A | Enable input to converter. Driving EN high or leaving this pin floating enables the converter. An external resistor divider can be used to implement an adjustable VIN UVLO function. |
VIN | 3 | P | Supply input pin to the internal LDO and high-side FET. Input bypass capacitors must be directly connected to this pin and GND. |
GND | 4 | G | Ground pin. Connected to the source of the low-side FET as well as the ground pin for the controller circuit. Connect to system ground and the ground side of CIN and COUT. The path to CIN must be as short as possible. |
SW | 5 | P | Switching output of the convertor. Internally connected to the source of the high-side FET and drain of the low-side FET. Connect to the power inductor. |
BST | 6 | P | Bootstrap capacitor connection for the high-side FET driver. Connect a high-quality, 100-nF ceramic capacitor from this pin to the SW pin. |
NC | 7 | A | Reserved pin. The user must leave this pin floating. |
FB | 8 | A | Output feedback input. Connect FB to the tap of an external resistor divider from the output to GND to set the output voltage. |