JAJSOG6 October 2022 TPS568231
PRODUCTION DATA
The TPS568231 has a MODE pin that can offer 12 different states of operation as a combination of current limit, switching frequency, and light load operation. The device can operate at two different current limits, ILIM-1 and ILIM, to support an output continuous current of 8 A, respectively.
The TPS568231 is designed to compare the valley current of the inductor against the current limit thresholds so make sure to understand that the output current is half the ripple current higher than the valley current. Take the ILIM current limit selection as an example. The OCL threshold is 8-A minimum, which means that a pk-pk inductor ripple current of 2-A minimum is needed to draw 9 A out of the converter without entering an overcurrent condition.
The TPS568231 can operate at three different frequencies of 400 kHz, 800 kHz, and 1200 kHz and also can choose between Eco-mode and FCCM mode. In Eco-mode, TPS568231 works in DCM (discontinuous conduction mode) with high efficiency in light loading, In FCCM mode, TPS568231 works in forced PWM (forced continuous conduction mode) with tight output voltage ripple. The device reads the voltage on the MODE pin during start-up and latches onto one of the MODE options listed in Table 7-2. The voltage on the MODE pin can be set by connecting this pin to the center tap of a resistor divider connected between VREG5 and AGND. A guideline for the top resistor (RM_H) and the bottom resistor (RM_L) in 1% resistors is shown in Table 7-2. Make sure that the voltage for the MODE pin is derived from the VREG5 rail only because internally this voltage is referenced to detect the MODE option. The MODE pin setting can be reset only by a VIN power cycling.
RM_L (kΩ) | RM_H (kΩ) | Light Load Operation | Current Limit | Frequency (kHz) |
---|---|---|---|---|
5.1 | 300 | FCCM | ILIM-1 | 400 |
10 | 200 | FCCM | ILIM | 400 |
20 | 160 | FCCM | ILIM-1 | 800 |
20 | 120 | FCCM | ILIM | 800 |
51 | 200 | FCCM | ILIM-1 | 1200 |
51 | 180 | FCCM | ILIM | 1200 |
51 | 150 | DCM | ILIM-1 | 400 |
51 | 120 | DCM | ILIM | 400 |
51 | 91 | DCM | ILIM-1 | 800 |
51 | 82 | DCM | ILIM | 800 |
51 | 62 | DCM | ILIM-1 | 1200 |
51 | 51 | DCM | ILIM | 1200 |
Figure 7-1 shows the typical start-up sequence of the device after the EN pin voltage crosses the EN turn-on threshold. After the voltage on VREG5 pin crosses the rising UVLO threshold, it takes 144 μs to read the first MODE setting and maximum approximately 180 μs from accomplishing MODE to soft start. The output voltage starts ramping after the MODE setting reading is completed.