JAJSHY7B September 2019 – August 2020 TPS61023
PRODUCTION DATA
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | FB | I | Voltage feedback of adjustable output voltage |
2 | EN | I | Enable logic input. Logic high voltage enables the device. Logic low voltage disables the device and turns it into shutdown mode. |
3 | VIN | I | IC power supply input |
4 | GND | PWR | Ground pin of the IC |
5 | SW | PWR | The switch pin of the converter. It is connected to the drain of the internal low-side power MOSFET and the source of the internal high-side power MOSFET. |
6 | VOUT | PWR | Boost converter output |