JAJSVH7A October 2024 – November 2024 TPS61287
PRODUCTION DATA
The TPS61287 has an internal cycle-by-cycle current limit to prevent the inadvertent application of a large switching current. Current limit detection occurs during the off-time by sensing of the voltage drop across the integrated high-side MOSFET. The high-side MOSFET is turned off immediately as soon as the switch valley current triggers the limit threshold. The switch valley current limit can be set by a resistor from the ILIM pin to ground. The relationship between the valley current limit and the resistor is shown in Equation 3.
where
For instance, the valley current limit is 20A if the RLIM is 20kΩ . ILIM pin can not be left floating or connected to VCC.