JAJSJL3C August 2020 – March 2022 TPS61288
PRODUCTION DATA
The output voltage is set by an external resistor divider (R1, R2 in the Figure 9-1 circuit diagram). For the best accuracy, R2 should be smaller than 300 kΩ to ensure the current flowing through R2 is at least 100 times larger than the FB pin leakage current. Changing R2 towards a lower value increases the immunity against noise injection. When R2 is higher than 15 kΩ, TI recommends adding a 27-pF ceramic capacitor (C6 in the Figure 9-1) in parallel with the R2 for noise immunity.
The value of R1 is then calculated as: