JAJSMG2C November 2023 – October 2024 TPS6287B10 , TPS6287B15 , TPS6287B20 , TPS6287B25 , TPS6287B30
PRODUCTION DATA
If you change the output voltage setpoint while the DC/DC converter is operating, the device ramps up or down to the new voltage setting in a controlled way.
The VRAMP[1:0] bits in the CONTROL1 register set the slew rate when the device ramps from one voltage to another during DVS (see Table 8-9).
VRAMP[1:0] | DVS Slew Rate |
---|---|
0b00 | 10mV/μs |
0b01 | 5mV/μs |
0b10 (default) | 1.25mV/μs |
0b11 | 0.5mV/μs |
Note that ramping the output to a higher voltage requires additional output current, so that during DVS the converter must generate a total output current given by:
where:
For correct operation, make sure that the total output current during DVS does not exceed the current limit of the device.