JAJSPL9 july 2023 TPS631012 , TPS631013
PRODMIX
The EN pin enables and disables the device.
The CONVERTER_EN bit in the Register CONTROL1 can also be used to enable and disable the output of the converter.
EXTERNAL EN PIN | INTERNAL EN (CONVERTER_EN) | DEVICE STATE | OUTPUT STATE |
---|---|---|---|
0 | X | Device in Shutdown | No Output |
1 | 0 | Programming Interface Active | No Output |
1 | 1 | Device Active | Output Enabled |
Note that when the EN pin is connected to logic low, all the I2C registers are cleaned and reset to the default values. While setting CONVERTER_EN to 0 has no influences on the I2C registers