JAJSF84B December 2008 – May 2018 TPS650250
PRODUCTION DATA.
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
SWITCHING REGULATOR SECTION | |||
AGND1 | 31 | — | Analog ground connection. All analog ground pins are connected internally on the chip. |
AGND2 | 13 | — | Analog ground connection. All analog ground pins are connected internally on the chip. |
Thermal pad | — | — | Connect the power pad to analog ground. |
VINDCDC1 | 5 | I | Input voltage for VDCDC1 step-down converter. This must be connected to the same voltage supply as VINDCDC2, VINDCDC3 and VCC. |
L1 | 6 | — | Switch pin of VDCDC1 converter. The VDCDC1 inductor is connected here. |
VDCDC1 | 8 | I | VDCDC1 feedback voltage sense input, connect directly to VDCDC1. |
PGND1 | 7 | — | Power ground for VDCDC1 converter. |
VINDCDC2 | 28 | I | Input voltage for VDCDC2 step-down converter. This must be connected to the same voltage supply as VINDCDC1, VINDCDC3 and VCC. |
L2 | 27 | — | Switch pin of VDCDC2 converter. The VDCDC2 inductor is connected here. |
VDCDC2 | 25 | I | VDCDC2 feedback voltage sense input, connect directly to VDCDC2. |
PGND2 | 26 | — | Power ground for VDCDC2 converter. |
VINDCDC3 | 4 | I | Input voltage for VDCDC3 step-down converter. This must be connected to the same voltage supply as VINDCDC1, VINDCDC2 and VCC. |
L3 | 3 | — | Switch pin of VDCDC3 converter. The VDCDC3 inductor is connected here. |
VDCDC3 | 1 | I | VDCDC3 feedback voltage sense input, connect directly to VDCDC3. |
PGND3 | 2 | — | Power ground for VDCDC3 converter. |
Vcc | 29 | I | Power supply for digital and analog circuitry of DCDC1, DCDC2 and DCDC3 DC-DC converters. This must be connected to the same voltage supply as VINDCDC3, VINDCDC1 and VINDCDC2. |
DEFDCDC1 | 9 | I | Input signal indicating default VDCDC1 voltage, 0 = 2.8V, 1 = 3.3V . |
This pin can also be connected to a resistor divider between VDCDC1 and GND. In this case the output voltage of the DCDC1 converter can be set in a range from 0.6V to VINDCDC1. | |||
DEFDCDC2 | 22 | I | Input signal indicating default VDCDC2 voltage, 0 = 1.8V, 1 = 2.5V . |
This pin can also be connected to a resistor divider between VDCDC2 and GND. In this case the output voltage of the DCDC2 converter can be set in a range from 0.6V to VINDCDC2. | |||
DEFDCDC3 | 32 | I | This pin must be connected to a resistor divider between VDCDC3 and GND. The output voltage of the DCDC3 converter can be set in a range from 0.6V to VINDCDC3. |
EN_DCDC1 | 20 | I | VDCDC1 enable pin. A logic high enables the regulator, a logic low disables the regulator. |
EN_DCDC2 | 19 | I | VDCDC2 enable pin. A logic high enables the regulator, a logic low disables the regulator. |
EN_DCDC3 | 18 | I | VDCDC3 enable pin. A logic high enables the regulator, a logic low disables the regulator. |
LDO REGULATOR SECTION | |||
VINLDO | 15 | I | Input voltage for LDO1 and LDO2. |
VLDO1 | 16 | O | Output voltage of LDO1. |
VLDO2 | 14 | O | Output voltage of LDO2. |
EN_LDO | 17 | I | Enable input for LDO1 and LDO2. Logic high enables the LDOs, logic low disables the LDOs. |
EN_Vdd_alive | 24 | I | Enable input for Vdd_alive LDO. Logic high enables the LDO, logic low disables the LDO. |
Vdd_alive | 12 | O | Output voltage for Vdd_alive. |
FB_LDO1 | 11 | I | Feedback pin for LDO1. |
FB_LDO2 | 10 | I | Feedback pin for LDO2. |
CONTROL AND I2C SECTION | |||
MODE | 23 | I | Select between Power Safe Mode and forced PWM Mode for DCDC1, DCDC2 and DCDC3. In Power Safe Mode PFM is used at light loads, PWM for higher loads. If PIN is set to high level, forced PWM Mode is selected. If Pin has low level, then Device operates in Power Safe Mode. |
PWRFAIL | 21 | O | Open drain output. Active low when PWRFAIL comparator indicates low VBAT condition. |
PWRFAIL_SNS | 30 | I | Input for the comparator driving the /PWRFAIL output. |