JAJSCK0 October 2016 TPS65266-1
PRODUCTION DATA.
PIN | DESCRIPTION | |
---|---|---|
NO. | NAME | |
1 | AGND | Analog ground pin |
2 | AGND | Analog ground pin |
3 | AGND | Analog ground pin |
4 | PGOOD | An open-drain output; asserts low if output voltage of bucks beyond regulation range due to thermal shutdown, over-current, under-voltage, or ENx low. |
5 | VINQ | Input voltage of converter controller and reference power supply bias. TI recommends to connect a 1-µF capacitor from the pin to analog ground and put the capacitor as near as possible to this pin. |
6 | FB2 | Feedback Kelvin sensing pin for buck2 output voltage. Connect this pin to buck2 feedback resistor divider. |
7 | COMP2 | Error amplifier output and loop compensation pin for buck2. Connect a series resistor and capacitor to compensate the control loop of buck converter 2 with peak current PWM mode. |
8 | SS2 | Soft-start and tracking input for buck2 converter. An internal 5.5-µA pullup current source is connected to this pin. The soft-start time of buck2 can be programmed by connecting a capacitor between this pin and ground. |
9 | BST2 | Boot strapped supply to the high-side floating gate driver in buck2 converter. Connect a capacitor (47 nF recommended) from BST2 pin to LX2 pin. |
10 | LX2 | Switching node connection to the inductor and bootstrap capacitor for buck2 converter. The voltage swing at this pin is from a diode voltage below the ground up to VIN2 voltage. |
11 | PGND2 | Power ground connection of buck2. Connect PGND2 pin as close as practical to the (–) terminal of VIN2 input ceramic capacitor. |
12 | VIN2 | Input power supply for buck2. Connect VIN2 pin as close as practical to the (+) terminal of an input ceramic capacitor (10 µF suggested). |
13 | VIN3 | Input power supply for buck3. Connect VIN3 pin as close as practical to the (+) terminal of an input ceramic capacitor (10 µF suggested). |
14 | PGND3 | Power ground connection of buck3. Connect PGND3 pin as close as practical to the (–) terminal of VIN3 input ceramic capacitor. |
15 | LX3 | Switching node connection to the inductor and bootstrap capacitor for buck3 converter. The voltage swing at this pin is from a diode voltage below the ground up to VIN3 voltage. |
16 | BST3 | Boot strapped supply to the high-side floating gate driver in buck3 converter. Connect a capacitor (47 nF recommended) from BST3 pin to LX3 pin. |
17 | SS3 | Soft-start and tracking input for buck3 converter. An internal 5.5-µA pullup current source is connected to this pin. The soft-start time of buck3 can be programmed by connecting a capacitor between this pin and ground. |
18 | COMP3 | Error amplifier output and loop compensation pin for buck3. Connect a series resistor and capacitor to compensate the control loop of buck converter 3 with peak current PWM mode. |
19 | FB3 | Feedback Kelvin sensing pin for buck3 output voltage. Connect this pin to buck3 feedback resistor divider. |
20 | ROSC | Oscillator frequency programmable pin. Connect an external resistor to set the switching frequency. |
21 | AGND | Analog ground common to buck controllers and other analog circuits. It must be routed separately from high-current power grounds to the (–) terminal of bypass capacitor of input voltage VINQ. |
22 | FB1 | Feedback Kelvin sensing pin for buck1 output voltage. Connect this pin to buck1 feedback resistor divider. |
23 | COMP1 | Error amplifier output and loop compensation pin for buck1. Connect a series resistor and capacitor to compensate the control loop of buck converter 1 with peak current PWM mode. |
24 | SS1 | Soft-start and tracking input for buck1 converter. An internal 5.5-µA pullup current source is connected to this pin. The soft-start time of buck1 can be programmed by connecting a capacitor between this pin and ground. |
25 | BST1 | Boot strapped supply to the high-side floating gate driver in buck1 converter. Connect a capacitor (47 nF recommended) from BST1 pin to LX1 pin. |
26 | LX1 | Switching node connection to the inductor and bootstrap capacitor for buck1 converter. The voltage swing at this pin is from a diode voltage below the ground up to VIN1 voltage. |
27 | PGND1 | Power ground connection of buck1. Connect PGND1 pin as close as practical to the (–) terminal of VIN1 input ceramic capacitor. |
28 | VIN1 | Input power supply for buck1. Connect VIN1 pin as close as practical to the (+) terminal of an input ceramic capacitor (suggest 10 µF). |
29 | EN1 | Enable for buck1 converter. Float to enable. Can use this pin to adjust the input undervoltage lockup of buck1 with resistors divider. |
30 | EN2 | Enable for buck2 converter. Float to enable. Can use this pin to adjust the input undervoltage lockup of buck2 with resistors divider. |
31 | EN3 | Enable for buck3 converter. Float to enable. Can use this pin to adjust the input undervoltage lockup of buck3 with resistors divider. |
32 | GND | Ground pin |
— | Thermal PAD | No electric connection to any signal. Soldered to the ground in PCB for better thermal performance. |