The path formed from the input capacitor to the inductor and the PH5 pin should have short trace length. The same applies for the trace from the inductor to Schottky diode D2 to the output capacitor and the VBOOST pin. Connect the
negative pin of the input capacitor and the PGND5 pin together with short trace lengths.
The resistor divider for sensing the output voltage connects between the positive pin of the output capacitor and the GND pin (IC signal ground). Do not locate these components and their traces near any switching nodes or
high-current traces.
Connect the compensation network between the COMP5 pin and GND pin (IC signal ground).