JAJSIR5C October 2019 – October 2023 TPS65313-Q1
PRODUCTION DATA
The WD SPI events are defined as follows:
This event occurs after a SPI request by the MCU SPI to read the WD question value register (WD_QUESTION[3:0]).
If the SPI frame is not successfully transmitted (a SPI fault is detected), the WD question event does not occur.
The MCU can request the pending active question value at the start of the new WD Q&A sequence run, but this MCU request is not a required condition for achieving a correct WD answer. The MCU can calculate the expected question value by running a question-generation algorithm.
The response occurs with an MCU write access to the WD_ANSWER[7:0] bits in the WDT_ANSWER register.
Each WD question requires four WD answers (three answers during RESPONSE WINDOW 1 and one answer during RESPONSE WINDOW 2).
The WD_ANSW_CNT[1:0] value is at 0x3 when the WD enters RESPONSE WINDOW 1 and decrements by 1 for each received WD answer.
The WD answer occurs with an MCU write access to the WD_ANSWER[7:0] bits during an OPEN WINDOW.
WD_ANSW_CNT[1:0] value stays at 0x1.