JAJSIR5C October 2019 – October 2023 TPS65313-Q1
PRODUCTION DATA
The logic built-in self-test (LBIST) tests the following monitoring and protection circuits in the digital core:
The digital core LBIST implementation is using an at-speed capture cycle with a run time of approximately 1.7 ms.
In case of an LBIST failure, the device goes into the SAFE state, and the LBIST_CORE_ERR bit in the SAFETY_LBIST_ERR_STAT register is set.
The LBIST runs in the RESET state when the RESET state extension is in progress. The LBIST can also run in the other operating states by setting the LBIST_EN bit, if the system fault-response time can allow the total 1.7 ms (typical) of run time to occur. During the LBIST, the device cannot monitor the supply outputs or the system MCU with the ESM and the watchdog. When the LBIST is complete, the LBIST_DONE status bit is set and the LBIST_EN control bit in the SAFETY_LBIST_CTRL register is cleared.
When the LBIST is activated in the DIAGNOSTIC state, the device clears the DIAG_EXIT_MASK bit in the DEV_STAT2 register. The DIAGNOSTIC state time-out timer continues to run while the LBIST is in progress. To keep the device in the DIAGNOSTIC state, the system MCU must set the DIAG_EXIT_MASK bit after the LBIST completion.
When the LBIST is activated while the device is in the ACTIVE state or the SAFE state, the state of the ENDRV/nIRQ driver is latched. The state of the ENDRV/nIRQ drive is restored when the LBIST is complete.
The diagnostic test on the LBIST can run by setting the LBIST_DIAG_EN control bit. The test on the LBIST signature check is performed by modifying either the expected signature value, input data string modification or both to force an LBIST error. The LBIST_DIAG_EN bit is cleared when the LBIST diagnostic test is complete.
The Table 11-3 summarizes the consequences of the LBIST runs.
LBIST_EN(3) | LBIST_DIAG_EN(3) | LBIST_DONE (4) | LBIST_CORE_ERR | LBIST_DIAG_ERR | DEVICE STATE |
---|---|---|---|---|---|
0b | 0b | No change | No change | No change | No state change |
0b | 1b | 1b | No change | 0(1) | No state change |
0b | 1b | 1b | No change | 1b | SAFE |
1b | 0b | 1b | 0b(2) | No change | No state change |
1b | 0b | 1b | 1b | No change | SAFE |