SLVSER3A November 2018 – April 2020 TPS65982BB
PRODUCTION DATA.
The unique-address interface allows for complex interaction between an I2C master and a single TPS65982BB device. The I2C slave sub-address is used to receive or respond to the protocol commands of the host interface. Figure 17 and Figure 18 show the write and read protocol for the I2C slave interface. Figure 19 provides a key to explain the terminology used. The key to the protocol diagrams is in the SMBus specification and is repeated here in part.