JAJSJU6 September 2020 TPS65982DMC
PRODUCTION DATA
Figure 8-2 shows the configuration when the TPS65982DMC is acting as a sink for the external switch path without an RSENSE resistor. In this mode, current is sunk from ADP_IN to an internal system power node, referred to as PP_EXT. To block reverse current, the ADP_IN and SENSEP pins monitor the voltage across the NFETs. To ensure that SENSEN does not float, tie SENSEP to SENSEN in this configuration. When configured in this mode, the digital readout from current from the ADC will be approximately zero.