JAJSJU6 September 2020 TPS65982DMC
PRODUCTION DATA
Figure 8-1 shows the configuration when the TPS65982DMC is acting as a sink for the external switch path. The external FETs must be connected in a common-drain configuration and will not work in a common source configuration. In this mode, current is sourced from ADP_IN. RSENSE provides an accurate current measurement and is used to initiate the current limiting feature of the external power path. The voltage between SENSEP (PP_EXT) and SENSEN (ADP_IN) is sensed to block reverse current flow. This measurement is also digitally readable via the ADC.