JAJSJU6 September 2020 TPS65982DMC
PRODUCTION DATA
The UFP Source port is the only DRP port that may connect as a DFP or UFP which means that it should have at least one sink capability when connected as a UFP. The DFP ports can only connect as a DFP, where they do not have any sink capabilities.
Port |
PDO Types |
Voltage |
Current |
---|---|---|---|
Port A |
Fixed |
5 V |
0 A |