JAJSJU6 September 2020 TPS65982DMC
PRODUCTION DATA
The TPS65982DMC Power Management block receives power and generates voltages to provide power to the TPS65982DMC internal circuitry. These generated power rails are LDO_3V3, LDO_1V8A, and LDO_1V8D. LDO_3V3 is also a low power output to load flash memory. VOUT_3V3 is a low power output that does not power internal circuitry that is controlled by application code and can be used to power other ICs in some applications. The power supply path is shown in Figure 8-7.
The TPS65982DMC is powered from either VIN_3V3 or ADP_IN. The normal power supply input is VIN_3V3. In this mode, current flows from VIN_3V3 to LDO_3V3 to power the core 3.3-V circuitry and the 3.3-V I/Os. A second LDO steps the voltage down from LDO_3V3 to LDO_1V8D and LDO_1V8A to power the 1.8-V core digital circuitry and 1.8-V analog circuits. When VIN_3V3 power is unavailable and power is available on ADP_IN, the TPS65982DMC will be powered from ADP_IN. In this mode, the voltage on ADP_IN is stepped down through an LDO to LDO_3V3. Switch S1 in Figure 8-7 is unidirectional and no current will flow from LDO_3V3 to VIN_3V3 or VOUT_3V3.