JAJSJU6 September 2020 TPS65982DMC
PRODUCTION DATA
The I2C connection from the PD controllers and the Dock Management Controller communicates to boot up the PD controllers and enable the Connection & Power Manager functions. The DMC has two GPIO dedicated for Port A/B and Port C/D interrupts. The shared interrupt connection to the Dock Management Controller will query both port addresses and will determine which port has been updated.
Table 9-6 shows and example of the port I2C address for each of the PD controller ports.
Port |
I2C Address |
---|---|
Port A |
0x20 |
Port B |
0x24 |
Port C |
0x21 |
Port D |
0x25 |