JAJSJU6 September 2020 TPS65982DMC
PRODUCTION DATA
At power-up, when VIN_3V3 is not present and ADP_IN is present, The TPS65982DMC will power itself from the ADP_IN rail (see Power Management) and execute boot code (see Boot Code). The boot code will observe the ADP_POWER_CFG voltage, which will fall into one of two voltage ranges: VBPZ_DIS, and VBPZ_EXT (defined in ADP_POWER_CFG Configuration Requirements).
When the voltage on ADP_POWER_CFG is in the VBPZ_DIS range (when ADP_POWER_CFG is tied to LDO_3V3 as in Figure 8-3), this indicates that the TPS65982DMC will not close the adapter power switch and route ADP_IN to the entire system. In this case, the TPS65982DMC will load SPI-connected flash memory and execute this application code.
The ADP_POWER_CFG pin can also alternately configure the TPS65982DMC to power the entire system through the adapter power switch when the voltage on ADP_POWER_CFG is in the VBPZ_EXT range (when ADP_POWER_CFG is tied to GND as in Figure 8-4).