JAJSJU7B September 2020 – October 2022 TPS65987DDK
PRODUCTION DATA
The UFP Source port is the only DRP port that may connect as a DFP or UFP which means that it should have at least one sink capability when connected as a UFP. The DFP ports can only connect as a DFP, where they do not have any sink capabilities.
PORT |
PDO TYPES |
VOLTAGE |
CURRENT |
---|---|---|---|
Port A |
Fixed |
5 V |
0 A |