JAJS425J October 2002 – May 2019 TPS795
PRODUCTION DATA.
Using the thermal metrics ΨJT and ΨJB, as shown in Thermal Information, the junction temperature can be estimated with corresponding formulas (given in Equation 6). For backwards compatibility, an older θJC,Top parameter is also listed.
where
NOTE
Both TT and TB can be measured on actual application boards using a thermo‐gun (an infrared thermometer).
For more information about measuring TT and TB, see the application note SBVA025, Using New Thermal Metrics, available for download at www.ti.com.
As shown in Figure 30, the new thermal metrics (ΨJT and ΨJB) have little dependency on board size. That is, using ΨJT or ΨJB with Equation 6 is a good way to estimate TJ by simply measuring TT or TB, regardless of the application board size.
For a more detailed discussion of why TI does not recommend using θJC(top) to determine thermal characteristics, see the application report SBVA025, Using New Thermal Metrics, available at www.ti.com.
For further information, see the application report SPRA953, IC Package Thermal Metrics, also available on the TI website.