JAJSRB5A September 2023 – November 2023 TPS7B4256-Q1
PRODUCTION DATA
The device has an internally fixed undervoltage lockout (UVLO) threshold. Undervoltage lockout activates when the input voltage VIN drops below the undervoltage lockout level (see the VUVLO(FALLING) parameter in the Electrical Characteristics table). This activation makes sure that the regulator is not latched into an unknown state during a low input supply voltage. If the input voltage has a negative transient that drops below the UVLO threshold and recovers, the regulator shuts down and powers up in the standard power-up sequence when the input voltage recovers to the required level (see the VUVLO(RISING) parameter in the Electrical Characteristics table).