JAJSVD1 September 2024 TPS7C84-Q1
ADVANCE INFORMATION
VOUT is set by the external feedback resistors R1 and R2, according to the following equation:
In this equation, VFB is the FB pin current error term. To ignore VFB in this equation, set the feedback divider current to 100 times the FB pin current listed in the Electrical Characteristics table. This setting provides the maximum feedback divider series resistance, as shown in the following equation: