SLUSCZ1 May 2017 TPS92518-Q1
PRODUCTION DATA.
The Read Response frame has the following format. The read response frame contains the state of the four fault bits. A special command is not required to poll the status of the bits, they are returned in every read response.
This is shown in Figure 35 below. This frame is sent out by the TPS92518-Q1 following a read command.