JAJSNQ5 may 2023 TPS92629-Q1
PRODUCTION DATA
The TPS92629-Q1 device provides two current output paths for each channel. Current flows from the supply through the R(SNS) resistor into the integrated current regulation circuit and to the LEDs through OUT pin and RES pin. The current output on both OUT pin and RES pin is independently regulated to achieve total required current output. The summed current of OUT and RES is equal to the current through the R(SNSx) resistor in the channel. The OUT connects to anode of LEDs load in serial directly, however RES connects to the LEDs through an external resistor to share part of the power dissipation and reduce the thermal accumulation in TPS92629-Q1.
The integrated independent current regulation in TPS92629-Q1 dynamically adjusts the output current on both OUT and RES output to maintain the stable summed current for LED. The TPS92629-Q1 always regulates the current output to the RES pin as much as possible until the RES current path is saturated, and the rest of required current is regulated out of the OUT. As a result, the most of the current to LED outputs through the RES pin when the voltage dropout is large between SUPPLY and LED required total forward voltage. In the opposite case, the most of the current to LED outputs through the OUT pin when the voltage headroom is relative low between SUPPLY and LED required forward voltage.