JAJSHS0C March 2019 – March 2021 TPS92682-Q1
PRODUCTION DATA
The ILED Undercurrent (UC) is a diagnostic feature and not a fault event. Therefore, the UC event sets the fault read bits in the FLT2 register only, and does not have any effect on the operation of the associated channel or trigger the fault pins.
The device sets the UC event when the voltage at the output of the current sense amplifier decreases by 50% from the regulation set point VIADJ. The UC threshold is calculated as follows:

When PWM dimming, the UC fault read bit might be set during the time when PWM is low.