JAJSHS0C March 2019 – March 2021 TPS92682-Q1
PRODUCTION DATA
The Write Response frame has the following format:
This is shown in Figure 7-25. This frame is sent out following a write command if the previously received frame was a write command and no SPI Error occurred during that frame.
The data and address bits in the write response are the data and address that were sent in the previous write command.